Hi,
My customer think that to use "-symdebug:coff" option on C667x device.
Because they want to COFF debugging with "-symdebug:coff" option.
They tried "-mv62" and "-mv67x+" option at their program.
"-mv62" is seems to work without problems, but "-mv67x+" does not work correctly.
I'm concerned about the following things:
Q1: Does C66 device is possible to use "-mv67x+" option?
Q2: Do you have any information in order to using the "-mv67x+" option on C66 device.
Best regards
H.U