n previous compile, there are two type of symbols, one start with underscore(_) that represents 32bits code or variables; the other start with dollars($) that represent 16bit code.
But from map file generated from the new compiler, all of the symbols only with underscore, but without any $. Could you please tell me the reason?
Map file:
00000060 _init_dpwm0
000000f4 _init_dpwm1
00000178 _init_dpwm2
000001e4 _init_dpwm3