Hi,
I'm currently working on a C2000 platform using the 6.2.11 compiler. I've been using the DWARF (-g) debug option for a while and everything was fine. I looked at the debug info in the OUT file and I can't find which dwarf version is being used. On another project, using ARM based TMS570, I can choose the dwarf version, be it 3 or 2. Is it possible to know which Dwarf version is used with the C2000 -g option?
Also, is there a difference in the generated dwarf from the ARM compiler and the C2000 compiler?
Last of all, I saw in the roadmap that ELF will be supported this summer in the next code generation tools for C2000. Will that bring the latest dwarf version? Will it the debug info generated with the C2000 compiler be the same as the ones from the ARM compiler?
Thanks in advance for your help.
Best regards,