Apologies if this seems a redundant query. I searched and I think this is new to the forum.
Within CCS 6.1 and with the eZ5535 DSP kit, I am trying to build code originally written for the C5505. I know about the I2S2 and the AIC3204 codec updates.
This is a compiler error with the following message. All source code .c files give this error. There are eight of them in my project. So, the error repeats 8 times.
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../aic3204.c'
'Invoking: C5500 Compiler'
"C:/ti/ccsv6/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=huge -O1 --symdebug:coff --include_path="C:/ti/ccsv6/tools/compiler/c5500_4.4.1/include" --include_path="C:/c55_lp/c55_dsplib_3.00" --include_path="C:/Users/Shankara/workspace_v6_1/FFT Example/project/Debug" --include_path="C:/Program Files (x86)/Texas Instruments/bios_5_41_10_36/packages/ti/rtdx/include/c5500" --include_path="C:/Users/Shankara/workspace_v6_1/FFT Example/project/Debug" --include_path="C:/Program Files (x86)/Texas Instruments/bios_5_41_10_36/packages/ti/bios/include" --define="_DEBUG" --define="C55X" --define=c5535 --diag_warning=225 --sat_reassoc=off --ptrdiff_size=32 --fp_reassoc=off --algebraic --no_mac_expand --asm_source=mnemonic --preproc_with_compile --preproc_dependency="aic3204.pp" "../aic3204.c"
ERROR: -v is not used by this program
ERROR! : unrecognized option [-v5515] (ignored)
ERROR! : Cannot open source file 74: No such file or directory
>> Compilation failure
gmake: *** [aic3204.obj] Error 1
Thanks!!!