I am using C2000 compiler version 6.2.11.
The compiler is generating the above error for memset()
The issue I am having is similar .
However, for that issue I was able to change the data type the table accepted.
For the current issue I am not able to do that. Also, casting the pointer to (void *) doesn't work.
Does anyone have a solution for this problem?
Note: I could store the pointer into a another void * variable and use that variable in the memset, however, I was wanting to know if there was another way to solve the problem.
Stephen