Hello,
My customer compile their project used by CCSv5. The project is also compiled on CCSv3.
Now they compare hex file of CCSv3 and v5, and memory address is difference like a following.
【CCSv3】0040 0000 ~ 0041 7FFF (Address range 96KB)
【CCSv5】0000 0000 ~ 0001 BFFF (Address range 112KB)
On hex file of CCSv5, the address 0000 0200 to 0000 7200 is not located anything, and 0040 0000 offset is not there.
Do anyone know the reason and how to resolve it?
Compiler version is as below.
【CCSv3】Ver3.2.2
【CCSv5】Ver4.4 (C5500compiler)
I attached both hex file.
Regards,
Kengo Furuya