When I compile with CCS5 I get several errors of type #20 identifier "MyUpmNum" is undefined. What does #20 refer to? Is there a numbered list of error descriptions that I can refer to get further information?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When I compile with CCS5 I get several errors of type #20 identifier "MyUpmNum" is undefined. What does #20 refer to? Is there a numbered list of error descriptions that I can refer to get further information?
Most CCS projects use the compiler build option --display_error_number. When this option is used, the compiler emits a unique ID number with every diagnostic. You can use these ID numbers to do things like change the level or disable specific diagnostics. See more about this in the Compiler Diagnostics slides from the compiler tips and tricks presentations. A full list of the diagnostics and their ID numbers can be found here.
Thanks and regards,
-George