Using the same CCS project and the same Compiler version CGT6000 TI v7.4.4 lead to different output on CCS 6.1.0 and CCS 5.5.0. The project generated by CCS 6.1.0 is about 60% larger.
I checked the compiler and linker flags and they are identical with respect of the library paths (ccsv6 instead of ccsv5). From my point of view the output should be the same using the same CGT version... I am wondering what else can be different?
Some additional information on the project:
- Using DSP/BIOS support version 5.42.1.09
- Output format: legacy COFF
- Project uses templates
Regards Tobias