Hello,
The code shown below is producing the assembly code shown below it. Why is the GpioCtrlRegs.GPAMUX1.... appearing in the assembly code?
Also, when I step through the code I noticed the bits are not set (as viewed in either the memory or expression's window. Why?
Stephen
Update: I forgot to mention that I am using the F283x CPU Cycle Accurate Simulator.
EALLOW; GpioDataRegs.GPASET.bit.GPIO0 = 1; GpioDataRegs.GPASET.bit.GPIO1 = 1; GpioDataRegs.GPASET.bit.GPIO2 = 1; GpioDataRegs.GPASET.bit.GPIO3 = 1; GpioDataRegs.GPASET.bit.GPIO4 = 1; GpioDataRegs.GPASET.bit.GPIO5 = 1; GpioDataRegs.GPASET.bit.GPIO6 = 1; GpioDataRegs.GPASET.bit.GPIO7 = 1; GpioDataRegs.GPASET.bit.GPIO10 = 1; GpioDataRegs.GPASET.bit.GPIO11 = 1; GpioDataRegs.GPASET.bit.GPIO12 = 1; GpioDataRegs.GPASET.bit.GPIO13 = 1; GpioDataRegs.GPASET.bit.GPIO14 = 1;
0099a5: 7622 EALLOW 0099a6: 761F01BF MOVW DP, #0x1bf 39 GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0; 0099a8: 8F006F80 MOVL XAR4, #0x006f80 16 GpioDataRegs.GPASET.bit.GPIO0 = 1; 0099aa: 1A020001 OR @0x2, #0x0001 39 GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0; 0099ac: 83A4 MOVL XAR5, @XAR4 17 GpioDataRegs.GPASET.bit.GPIO1 = 1; 0099ad: 1A020002 OR @0x2, #0x0002 18 GpioDataRegs.GPASET.bit.GPIO2 = 1; 0099af: 1A020004 OR @0x2, #0x0004 19 GpioDataRegs.GPASET.bit.GPIO3 = 1; 0099b1: 1A020008 OR @0x2, #0x0008 39 GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0; 0099b3: DD06 ADDB XAR5, #6 20 GpioDataRegs.GPASET.bit.GPIO4 = 1; 0099b4: 1A020010 OR @0x2, #0x0010 21 GpioDataRegs.GPASET.bit.GPIO5 = 1; 0099b6: 1A020020 OR @0x2, #0x0020 22 GpioDataRegs.GPASET.bit.GPIO6 = 1; 0099b8: 1A020040 OR @0x2, #0x0040 23 GpioDataRegs.GPASET.bit.GPIO7 = 1; 0099ba: 1A020080 OR @0x2, #0x0080 26 GpioDataRegs.GPASET.bit.GPIO10 = 1; 0099bc: 1A020400 OR @0x2, #0x0400 27 GpioDataRegs.GPASET.bit.GPIO11 = 1; 0099be: 1A020800 OR @0x2, #0x0800 28 GpioDataRegs.GPASET.bit.GPIO12 = 1; 0099c0: 1A021000 OR @0x2, #0x1000 29 GpioDataRegs.GPASET.bit.GPIO13 = 1; 0099c2: 1A022000 OR @0x2, #0x2000 30 GpioDataRegs.GPASET.bit.GPIO14 = 1; 0099c4: 1A024000 OR @0x2, #0x4000