For TI C64x+ and the compiler is ti-cgt-c6000_8.0.1, i want to know whether the compiler is using the already linked ELF FastRTS library or is it using the default ELF RTS library. Can you please provide me with some method by which i can verify the same?
In the .map file i can see both ELF RTS and ELF FastRTS .obj files, but I want to confirm that my FastRTS library is working fine and the compiler is prioritising it over the RTS library.