Hi there,
I wanted to use MATLAB R2015a to control BLDC motor with TI LaunchPad F28069M with the BoosterPack. I have done already all instalations needed, have CCSV5, controlSUITE, supportpackage for MATLAB and TI C2000, and have tried so many compilers, 15.6.0, 6.4.6, 6.0.2., 6.2.5. and many others. But it always ended up with this:
Debug Assertion Failed!
Program: C:\ti\ccsv5\tools\compiler\c2000_1\bin\cI2000.exe
File:isctype.c
Line:56
Expression: (unsigned)(c+1)<=256
and in the Diagnostic Viewer with this:
INTERNAL ERROR: C:/ti/ccsv5/tools/compiler/c2000/bin/cl2000 had an internal inconsistency and aborted while processing file C:/ti/c28069pmsmfocdual_ert_rtw/MW_c28xx_board.c This is caused by a defect in the compiler itself. TI Customer Support may be able to suggest a workaround to avoid this. Upgrading to the newest version of the compiler may fix this problem. Contact TI in the E2E support forums at http://e2e.ti.com ....
Does anybody please have any idea, what is wrong and how could it be fixed?
I would very appreciate it.
Thank you very much.