Hi, I am trying to run the dlmfast example from the TMS320C55x DSP Library. I use the C5517EVM board. When I build the project, I get the following error: Only --ptrdiff_size=32 is allowed for huge memory model. I have seen that there are similar post, but none of them helped me.
I have performed the following actions:
1. Imported Chip support library and one example runs perfectly
2. Imported the TMS320C55x DSP Library
3. Followed the installation guide from the following TI document: http://www.ti.com/lit/ug/spru422j/spru422j.pdf
a) Executed the file: Blt55xh_r3.bat
b) Placed the file 55xdsph_r3.lib in the runtime support library
4. Then I have built the dlmsfast project and got this error message in the CDT build console: ptrdiff_size=32 is allowed for huge memory model 5. I have tried to use other runtime support library files with different memory models. But maybe that is the wrong way to change the memory model? I suspect that I should use another memory model. However, which one? And how do I instruct the compiler to use another memory model?
I am quite new to this and will really appreciate some help:)