We are building an application for the OMAP-L138 with a C674x Fixed / Floating Point DSP (MityDSP) and using the C6000 build tools in CCS. We would like to be able to build identical output images from 2 different build machines. (i.e. one build for development another build for configuration management) What we have found is that there is a timestamp in the executable file image which is updated to the current time on the machine as well there are several 3 and 4 byte locations that differ between build instances. Is there a option/setting/switch to suppress the timestamp in the project output file? Essentially, what we want to achieve is to be able to create an executable output file change the name of that file and then create a new output file and using a binary comparison have the two files be identical.
Thanks in advance for looking into this question.