Hi All,
I have the following problem: I have to use the TMS470 v4.4.10.121 compiler. As I see, I can not download only the compiler directly and activate it. I have to download one of the CCS versions, which contains a TMS compiler, and activate the CCS. Without the CCS the Compiler can not be activated, right? Which CCS Version shall I download, to be able to licence the 4.4.10.121 Compiler? I do not really understand how this works.
Regards,
Szabolcs