Hi,
I have a C++ project in Windows, MSVC, which uses vector, set header files. I want to port this project to AM3359 Starter Kit board. The build is OK. When debug it, after a step through at the first line code, a new tab pops up having error:
Can't find a source file at "/cbuild/slaves/oorts/crosstool-ng/builds/arm-linux-gnueabihf-linux/.build/arm-linux-gnueabihf/build/build-cc/arm-linux-gnueabihf/libstdc++-v3/include/bits/allocator.h"
Locate the file or edit the source lookup path to include its location.
Here is the C++ code:
#include "Query.h" #include "TextQuery.h" #include <string> #include <set> #include <iostream> using std::set; using std::string; using std::cin; using std::cout; using std::cerr; using std::endl; int main(int, char **argv) { TextQuery file = build_textfile(argv[1]);
Could you tell me how to remove the debug error?
Thanks,