I am working with CCS v6.1. Where do I find rts6740.lib and how to download?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am working with CCS v6.1. Where do I find rts6740.lib and how to download?
RTS support libraries like rts6740.lib are part of the compiler package. They are not downloaded separately. They are located in a directory location similar to ...
C:\ti\ccsv6\tools\compiler\ti-cgt-c6000_8.0.3\lib
Thanks and regards,
-George
J Thanks said:he resolved it by recopying the 6740_elf.lib as rts6740.lib
I recommend against doing that. The names of the RTS libraries are special. rts6740_elf.lib is the EABI library, and rts6740.lib is supposed to be the COFF version. Most likely, the project refers to rts6740.lib directly; it should instead refer to libc.a