I have a project that successfully compiles and runs using the 6.2.9 Compiler. Target is a f28335 processor. I changed the Compiler to 6.4.x (I've tried several 6.4.4, 6.4.6, etc) and the project compiles, flashes to the chip but does not run. When I try to step through the processor, The first statement is a memcpy of some functions to RAM. It hangs on this statement. If I comment out the statement, it goes further before hanging on a function call (the debugger reports that it can't find the source file but the function is in the same file so the error makes no sense). What broke between the old compiler and the new compiler? Is there some setting that would need to be changed?
Thanks