Does the Ti ARM compiler in CCS support "#pragma once"? Is there a trick to turn it on? I am not seeing it working.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TI compiler does support #pragma once. What do you see which makes you think it doesn't work? What version of the compiler do you use?
Thanks and regards,
-George
Can you point to the documentation that shows support for this? I don't see it in the 15.12.0 compiler guide.
You are correct that #pragma once does not appear in the compiler manual. I filed CODEGEN-1678 in the SDOWP system to have this addressed. Feel free to follow it with the SDOWP link below in my signature.
Thanks and regards,
-George
An internet search on #pragma once returns many links that describe it. Every compiler that supports it does it the same way. It intended for use in header files. An appearance of #pragma once in a header file means that, should the header file be included multiple times, only the first one counts.
Thanks and regards,
-George
Please try this simple experiment. What follows is a header file, and a C source file.
// hdr.h #pragma once #warn only see this one time
// src.c #include "hdr.h" #include "hdr.h" int a;
When you compile src.c, it should look similar to this ...
%> armcl src.c "hdr.h", line 3: warning: #warn directive: only see this one time
Even though hdr.h is included twice, the #warn diagnostic is emitted only once. What happens when you try this experiment?
Thanks and regards,
-George