Hello,
I have a lib in IAR that I want to use in CCS - I am seeing the following errors I was hoping to get some help with:
error #16004-D: file "E:\Projects\_SVN\trunk\Code\FreeRTOS Example Projects\IAR\HDK_3137_IAR - 2 - Lib\Debug\Exe\HDK_3137_IAR.a<main_blinky.o>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("3"); combining incompatible files
error #16012-D: file "E:\Projects\_SVN\trunk\Code\FreeRTOS Example Projects\IAR\HDK_3137_IAR - 2 - Lib\Debug\Exe\HDK_3137_IAR.a<portASM.o>" does not preserve 8-byte alignment of 8-byte data, but other input files require this; incompatible files
error #16011-D: file "E:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/lib/rtsv7R4_A_be_v3D16_eabi.lib<memcmp.obj>" requires 8-byte alignment of 8-byte data, but not all input files preserve this; incompatible files
Thanks In Advance,
johnw