I would like to find the symbol address and symbol size of a symbol from the symbol table.(c28069 piccolo)
To generate symbol table, I have used the following commands
ofd2000 application.out
nm2000 -l application.out
Copy pasting some part of the symbol table below
Symbol Table
id name value kind section binding type
-- ---- ----- ---- ------- ------- ----
0 .vectors 0x00000000 defined .vectors local section
2 .text 0x003f5041 defined .text local section
4 .switch 0x00000000 defined .switch local section
As you can see, there is no field such as "size" to find the symbol size.
Both the commands provide me the symbol address, but I am unable to find the symbol size. (Earlier I have used ARM targets with GNU compiler, GNU provides a tool "arm-none-eabi-objdump" that provides both symbol table and symbol size)
Any suggestions on how to use the TI utilities to suffice my need? Or are they other utilities I need to be aware of?
Thanks in advance for the help,
Amit