Hi Champs ,
Our customer get the specification for in system programming which is need like the bellowing structure.
There will be two section for updating the new firmware.
Our question is the image should be able to work at section A and section B at the same time.
However, the location address will be defined when we build the image.
Is it possible to achieve that ? such like using the general register to be an offset and force the branch using indirect address
which we can control it by offset value to make it for section A and section B at the same time.
Thanks
BR
Brian