Hi,
I really appreciate cryptic error messages. So what does that really mean?
I just added a static member pointer to a class, which is called pThis.
"C:/ti/controlSUITE/device_support/f28m36x/v207/F28M36x_examples_Dual/mtoc_ipcdrivers_lite/c28/ccs/../../../../F28M36x_common/cmd/F28M36x_generic_wshared_C28_FLASH.cmd", line 156: remark:
undefined first referenced
object "GETBUFFER" is not allocated, but is being placed as part of
symbol in file
allocated object "GROUP_8"
--------- ----------------
"C:/ti/controlSUITE/device_support/f28m36x/v207/F28M36x_examples_Dual/mtoc_ipcdrivers_lite/c28/ccs/../../../../F28M36x_common/cmd/F28M36x_generic_wshared_C28_FLASH.cmd", line 157: remark:
f28M36x_c28::IpcCom::pThis ./Ipc_Com_c28.obj
object "GETWRITEIDX" is not allocated, but is being placed as part of
allocated object "GROUP_8"
error: unresolved symbols remain
"C:/ti/controlSUITE/device_support/f28m36x/v207/F28M36x_examples_Dual/mtoc_ipcdrivers_lite/c28/ccs/../../../../F28M36x_common/cmd/F28M36x_generic_wshared_C28_FLASH.cmd", line 158: remark:
error: errors encountered during linking; "mtoc_ipcdrivers_lite_c28.out" not
object "PUTREADIDX" is not allocated, but is being placed as part of
built
allocated object "GROUP_8"
gmake: *** [mtoc_ipcdrivers_lite_c28.out] Error 1
EDIT:
correction the error is generated after the following codeline was added to the constructor
IpcCom::IpcCom()
{
pThis = this;