Hi all,
I'm currently working on a project, using the MSP430F5438A.
I use a function which is fixed and written into Flash Memory. I would like to execute it from RAM, without using memory allocation of the RAM.
I've ever tried with ".function LOAD=Flash_Area RUN=Ram_Area" but during execution code, I have an issue with an assembly instruction BRA#???? I've created a post about this problem.
Does exist a specific pragma or another solution which could be useful for my problem ?
If someone would have an idea,
Regards