Hello,
We are using Code Composer Studio version 5.5 with the Code Generation Tools Compiler version 6.2.10. We have two PCs where on one machine we run a build with the IDE, and on the other, from the command line. These are identical source, identical files included, and identical parameters are used for compile settings.
The only difference is the binary generated from the PC using a command line driven build is about 10 kilobytes larger than the PC using the IDE to build the same. Naturally the checksums of each do not match which is what flagged our attention for this.
Can you offer any suggestions as to why we are experiencing this, given all the similarities between the two PC’s?
-Jim