Hi,
I am porting code from a 6713 to 28335 and I am getting this warning message, which I don't understand. Apparently something in one of the includes pulls in a header file called s_c__ti.h which is in conflict with something else. It happens on every file in the build. Any suggestions on how this file got included or why it is causing an error would be appreciated.
Thanks,
Lloyd
"C:\\ti-ccsv6\\ccsv6\\utils\\bin\\gmake" -k -j 8 all -O
'Building file: ../Source/uart.c'
'Invoking: C2000 Compiler'
"C:/ti-ccsv6/ccsv6/tools/compiler/c2000_15.12.3.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --include_path="C:/ti-ccsv6/ccsv6/tools/compiler/c2000_15.12.3.LTS/include" --include_path="C:/ti/controlSUITE/device_support/f2833x/v141/DSP2833x_common/include" --include_path="C:/ti/controlSUITE/device_support/f2833x/v141/DSP2833x_headers/include" --include_path="C:/ti-ccsv6/ccsv6/tools/compiler/c2000_15.12.3.LTS/include" --include_path="C:/Users/lslonim.ESLTEMP-DOMAIN/Documents/Arrestment/Software/AAG Code workspage v6/trunk/Dev2 28335 Diagnostics/Include" --advice:performance=all -g --display_error_number --diag_warning=225 --diag_wrap=off --preproc_with_compile --preproc_dependency="Source/uart.d" --obj_directory="Source" "../Source/uart.c"
"C:/ti-ccsv6/ccsv6/tools/compiler/c2000_15.12.3.LTS/include/s_c_features.h", line 439: warning #48-D: incompatible redefinition of macro "_STLP_VENDOR_CSTD" (declared at line 112 of "C:/ti-ccsv6/ccsv6/tools/compiler/c2000_15.12.3.LTS/include/s_c__ti.h")
'Finished building: ../Source/uart.c'
My headers are:
#include <stdlib.h>
#include <stdio.h>
#include <math.h>
#include <string.h>
#include <cstdarg>
#include "DSP2833x_Device.h"
#include "Types.h"
#include "globals.h"