This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to install CGT for C2000 and c6000 in CCS

Hello all,

I have installed the latest release of the CGT file for C2000 it to the following path: C:\ti\ccsv6\tools\compiler. Then after adding  the same directory in the compilers' option (Windows>Preferences>Code Composer Studio>Build>Compilers) and then clicking on the refresh there seemed to be no new compiler added to the list. Is this the process i should be following or am i doing something wrong. Kindly help. 

CCS v6.1.3.00034

Windows 7

TIA

  • I'm not familiar with the method you describe.  Please try the method described in this video.

    If that doesn't work out, then try one of the methods described in this wiki article.

    Thanks and regards,

    -George

  • Hey George thank you for the link. As shown in the video (after clicking 'show more') the compiler for C2000 was not visible on my version of CCS but when i selected 'All' instead of 'Relevance' (in the drop-down beside the search option) all the add-ons became visible.

    Thanks and Regards,
    Jyotirmaya
  • Hey George,

    I have now tried installing the compiler for C2000 as given in the above video but no luck so far. After the installation I checked the compiler tab in the preference menu and it does not show C2000 compiler in the list. Is it due to the CCS version being used?

    Thanks and Regards
    Jyotirrmaya
  • Please use the method describe here for seeing which versions of the compiler are recognized by CCS.  What versions of the compiler do you expect to see?  How does that differ from what you actually see?

    Thanks and regards,

    -George

  • Compiler version greater than 6.2.3 is required for my project. As per the method given in the above video after installing the C2000 compiler from the App Center a new folder is created in the following path C:\ti\ccsv6\tools\compiler with the filename as 'ti-cgt-c2000_16.6.0.STS'. After reopening CCS when I check the list of compilers installed (Windows>Preferences>Code Composer Studio>Build>Compilers) C2000 compiler is still not visible.

    So after that I uninstalled CCS and then selected all the required compilers (including C2000) in the setup process itself and everything seems to work fine now.

    Thanks a lot for your help George.

    Regards,
    Jyotirmaya