I'm using the secure boot, so there are some SK_API calls in my project.
I can build my project successfully with COFF output format.
But when I try to build the project with ELF output format, there is a error:
So I find the lib file in \ti\ccsv5\tools\compiler\c6000_7.4.4\lib,
there is a rts64plus_elf.lib and a rts64plus.lib.
I thought the rts64plus.lib is COFF format, and the rts64plus.lib is ELF format.
So, I changed the name of rts64plus_elf.lib to rts64plus.lib, and rebuild the project, but got:
So, I think the rts64plus_elf.lib doesn't have the SK_APIs.
I find the source code in the ti\ccsv5\tools\compiler\c6000_7.4.4\lib\
The rtssrc.zip is the package of the source code. And there is a mklib.exe. I tried the mklib.exe but it occured some errors. I've use mklib -h to see the options of the command, but didn't get the right way to compile the source code.
I've also open a new CCS "Static Library" project and add all the source files to the project. But when I build the project, many errors occured.
Can TI give me some guidance on recompile the source code?
And can TI provide me the rts64plus.lib in ELF format?
Thank you.
Frank