Dear All:
When I use CCS 6.2 to build the example project which is in the controlSUITE\device_support\f2803x\v130\DSP2803x_examples_cla_ccsv5\iir2p2z,
it works fine. But if I change the iir2p2z.cla file (add a space or new line, no code), It shows up a error #7: unrecognized token on line1,when I build it.
I have searched the forum, I can not get the answer. Please help. Thanks.