I see a ton of Unresolved Symbol posts but none seem to match my situation
I am creating some functions for my students to use (EE Freshman and Sophomores) in Code Composer Studio on the MSP432 Launchpad platform. I can create the .c and .h files. Place them in a separate directory, add the directory to the Project - Properties - Build - Compiler - Include Options path. I can see the directory and both .c and .h files in Project Explorer - MyProject - Includes. I #include the .h file in my current program and it finds the .h file and the function prototypes as evidenced by them showing up in the Outline window. When I compile I get the Unresolved Symbol error indicating
Description Resource Path Location Type
unresolved symbol Clock_Init_48MHz, first referenced in ./delay_check.obj myFirstProject C/C++ Problem
Which I assume means it cannot find the .c file.
A) What am I missing
B) What CCStudio document discusses this - I have looked at several and none go into this detail
thanks
tj