Tool/software: TI C/C++ Compiler
In the end of map file, there is a list of global symbols, list the address and name. some address is the real address of the symbol, but some is not address obviously, for example below the _STACK_SIZE is a const value set in cmd file.
GLOBAL SYMBOLS: SORTED BY Symbol Address
address name
------- ----
00001000 __STACK_SIZE
00001000 __SYSMEM_SIZE
in cmd file:
-stack 0x000001000 /* Stack Size */
-heap 0x000001000 /* Heap Size */
and also below value of symbol also should not be address:
ffff0000 INT_VECS
ffffffff ___binit__
ffffffff ___c_args__
ffffffff ___pinit__
ffffffff binit
ffffffff pinit
For BIOS based project, there will be more similar symbol as below picture. with same "address". Is this a real address, or just a const value? is there a explanation to the map file format?