Tool/software: TI C/C++ Compiler
Hi,I get the introduction of memory protection from the section 2.9.2 of TRM :sprufk5a-TMS320C674x DSP Megamodule, I set the memory protection register value as follow:
1、Enable L1P、L1D Cache 32K
2、MPPA
L1PMPPA0-31: 0,all access dennied。
L1DMPPA0-31: 0,all access dennied。
when I debug it,I found that write to L1P、L1D memory can trigger an exception PMC_CMPA /DMC_CMPA event ,but read from L1P 、L1D memory,there is no exception。
Is this right?