Other Parts Discussed in Thread: CONTROLSUITE, SFRA
Tool/software: TI C/C++ Compiler
Running the HV_1PH_DCAC/v1_04_00_00/f2837x/voltagesourceinverterlcfltr solution in controlSUITE.
When compiling the build level 3 options, as stated in the user's guide, there's a segmentation fault generated. Build levels 1 and 2 compiled with no issues. This seems to be an issue with v.16.9 as the example builds with older compilers. Error message below:
INTERNAL ERROR: C:\ti\ccsv6\tools\compiler\ti-cgt-c2000_16.9.0.LTS\bin\cg2000.exe experienced a segmentation fault
while processing function _inverterISR
This is caused by a defect in the compiler itself. TI Customer
Support may be able to suggest a workaround to avoid this.
Upgrading to the newest version of the compiler may fix this problem.
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue". Include this ENTIRE error message and a
copy of the .pp file created when option --preproc_with_comment
(-ppc) is used.
gmake: *** [voltagesourceinvlcfltr.obj] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****