• Not Answered

CCS/TMDSRM48HDK: Debug Call Stack - "next frame is identical to an existing frame"

Part Number: TMDSRM48HDK

Tool/software: Code Composer Studio

Hello,

I have some problems when debbuging with Code Composer Studio (6.1.2.00015).

I’m trying to get the functions call stack but there is only the previous frame repeated or the message « next frame is identical to an existing frame ».

I’m working with a RM48HDK (RM48L952ZWT rev E) board using a RTOS (µCOS-III) and I’m debbuging with a Spectrum Digital XDS200 USB debug probe. The host OS is Windows 7 Professional 64bits Service Pack 1.

These are my project settings :

Compiler :

-mv7R4 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.7/include" --display_error_number --diag_warning=225 --diag_wrap=off --enum_type=packed --no_stm

Linker :

-mv7R4 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me -g --display_error_number --diag_warning=225 --diag_wrap=off --enum_type=packed -z -m"MUX.map" --stack_size=0x800 --heap_size=0x800 -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.7/lib" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.7/include" --reread_libs --warn_sections --diag_wrap=off --display_error_number --xml_link_info="MUX_linkInfo.xml" --rom_model

Is there a way to see the complete call stack ? Is it a bug or do I need to put some parameters ?

Thanks,

Bastien

7 Replies