Other Parts Discussed in Thread: CC3200, ENERGIA
Tool/software: TI C/C++ Compiler
Hello everyone !
I'm not used to playing with C/C++ or even with compiled languages so maybe it'll be a dumb question but after a lot of research, I don't know what to do.
A bit of information about my environment :
- OS : Win 10
- CCS version : 6
- Compiler version : TI v16.9.3.LTS
As I need to use Free-RTOS, my project is based on the "freertos_demo" example from CC3200's examples. This is the project's structure :
I started my project using Energia and I wanted to use it inside this "freertos_demo" project. To do so, I needed to include Energia.h header.
The IDE recognizes well the methods, but when I compile I get this error :
I googled the error and found that the problem was due to some needed files not found by the linker.
The errors being all due to methods defined in Energia.h, I tried several ways to include it. After a few unsuccessfully attempts, I put it in the File Search Path like this :
With this, the error did disappear, but to be replaced by the following :
Now I am wondering: have I properly fixed my previous error and am I now facing a completely different issue ? Or are these two issues linked ?
I hope that I have given you enough information, please ask me if you need some more.
Thanks for reading me !