Tool/software: TI C/C++ Compiler
I'm trying to compile a TMS320TCI6614 project with the CGT 8.1.4(also tried 8.1.3, 8.2.0, 7.4.21), but in one of the files, the following error occurs
>> Compilation failure
Source/dft/scalar/codelets/subdir_rules.mk:357: recipe for target 'Source/dft/scalar/codelets/t2_64.obj' failed
>> ../Source/dft/scalar/codelets/t2_64.c, line 3808:
INTERNAL ERROR: >>>Register allocation failed: t2_64(int *, int
*, const int *, int, int, int, int)
This may be a serious problem. Please contact customer support with a
description of this problem and a sample of the source files that caused this
INTERNAL ERROR message to appear.
Cannot continue compilation - ABORTING!t2_64.pp.7z