Tool/software: TI C/C++ Compiler
Trying to add .cpp files in current project . When compiling one .cpp file CCS gives error for namespace (identifier "namepsace" is undefined ).
Code Composer Studio - Version: 6.2.0.00050 used.
Is C++ fully supported by CCS(6.2.0.00050) ?
If yes then what setting need to be done in CCS ? Already gone through the "http://processors.wiki.ti.com/index.php/C%2B%2B_Support_in_TI_Compilers".
If partially yes for C++ support ,which C++ Language Feature it does not support
Does it support features like Multiple Inheritance ,Virtual Base Classes, Namespaces,Exceptions, Templates ,Dynamic Casts