Tool/software: TI C/C++ Compiler
Hi,
I'm a little bit confused about the different compilers available to work on this board (TMDX570LC43HDK), considering for example:
- arm_15.12.6LTS from TI
- gcc-arm-none-eabi-6-2017-q2-update from ARM
which one is better to use and why considering as target board Hercules TMDX570LC43HDK ?
The gcc-arm-none-eabi-6-2017-q2-update is installed on the PC where I've CCSV6 but it is not recognized by CCSV6,
there is a way to choose this compiler in CCSV6?
It is possible to use TI compiler also outside of CCSV6 (I need to use it together with an hypervisor)?
Thanks
Antonio