Tool/software: Code Composer Studio
Specifically, the library file rtsv7A8_A_le_n_v3_eabi.lib is not getting built. I've perused the forums, this seems to be a somewhat common error, but I haven't run across the solution to the problem. If I simply copy the file rtsv7A8_A_le_n_v3_eabi.lib from my old PC that has CCS 5.4, then the build runs to completion so the lack of being able to build rtsv7A8_A_le_n_v3_eabi.lib is the only problem. I'm using xdc 3.24.5.48