This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28377D: ac2000 segmentation fault

Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE

Tool/software: TI C/C++ Compiler

The attached project has a simple main that causes a segmentation fault of compiler.

I think that the issue is related to any use of an array of size zero inside of an structure.

Code is the following:

void donothing(int* v)
{
}

template <int sz>
struct Myarray
{
    int v[sz];

    void func()
    {
        donothing(v);
    }
};


int main()
{
    Myarray<0> k;
    k.func();


}

And the error output is:


**** Build of configuration Debug for project SFault ****

"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 8 all -O
'Building file: ../main.cpp'
'Invoking: C2000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.6.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla1 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu2 --include_path="C:/Users/jbm/workspace_c2000ware/SFault" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.6.LTS/include" --advice:performance=all -g --preproc_only --preproc_with_comment --preproc_with_compile --preproc_with_line --diag_warning=225 --diag_wrap=off --display_error_number  "../main.cpp"

>> Compilation failure
subdir_rules.mk:9: recipe for target 'main.obj' failed

INTERNAL ERROR: C:\ti\ccsv7\tools\compiler\ti-cgt-c2000_16.9.6.LTS\bin\ac2000.exe experienced a segmentation fault
                  while processing function (unknown or file scope) file (unknown) line 0

This is caused by a defect in the TI C/C++ Parser.
TI Customer Support may be able to suggest a workaround to avoid this.

Upgrading to the newest version of the compiler may fix this problem.

Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler".  See the link titled
"Submitting an issue".

We need to see this ENTIRE error message and a complete, reproducable
test case including ALL of the command-line options.
Include the .pp file created by option --preproc_with_comment

gmake: *** [main.obj] Error 1
gmake: Target 'all' not remade because of errors.

**** Build Finished ****

Any workarround for this issue would be very appreciated, regards.