Tool/software: Code Composer Studio
Hi,
I have a code base that was built on CCS5.3 (Compiler:7.4.0). Now I wanted to migrate it to CCS7.2 (Compiler:8.1.3). When I try to build in CCS7.2, I get error saying cannot fit into memory. So I need to relocated some sections of my library and .text to DDR3 from L2SRAM in my lnk.cmd. All other settings are unchanged. Can some one please tell me why the .out files sizes differs and need to change lnk.cmd with the same code base??
Exact CCS Console:
error #10099-D: program
will not fit into available memory. run placement with alignment fails for
section "dpTemporaryWorkMemory_L2" size 0x1000 . Available memory ranges:
L2SRAM size: 0xecf00 unused: 0x7d max hole: 0x60
I dont want to change my lnk.cmd?? Is there a way to achieve that with CCS7.2 and Compiler:8.1.3.
Thanks
Pradeep