Tool/software: TI C/C++ Compiler
I have a function A located in file 1. This function is called two times in a function B located in file 2.
However, when function A is called, the input argument does not correspond to the parameter as set in function B.
What could be the issue? This code is obtained from an IC vendor - so it should presumably work without any modifications.
Thanks,
Tomas
B: the argument is 29747.
A: the input argument is 0.