Tool/software: TI C/C++ Compiler
Hi,
I have been having the following error when compiling one of our projects for C6657:
INTERNAL ERROR: C:\ti\ccsv5\tools\compiler\c6000_7.4.24\bin\cg6x.exe experienced a segmentation fault
I have not had the issue before, but it started happening recently. I suspect it is because some changes to our source code, maybe #inlcude got too deep, etc.
- I have tried compier 7.4.24, 7.4.23 and 7.4.2, but none worked.
- The strange thing is, the problem doesn't occur on other PCs. We use the same compiler, but somehow the problem seems to occur only my PC.
- Disabling the optimization works around the issue (originally set to 3, setting to off works around the issue).
I tried to create a minimum set of files which exhibits the issue, but this is a part of a large project, so it is very difficult.
Do you have any ides what is going on? Or do you know of any way to work around the issue?