Tool/software: Code Composer Studio
Hi,
I have build a code base in CCS5 and CCS7. Baring the compiler versions all other packages are same.
The .map file generated in both of the IDEs are different.
CCS7:
.cinit 0 00892778 00005ef0
00892778 00004d7c (.cinit..fardata.load) [load image]
CCS5:
.cinit 0 9f0ac30c 00002a4c
9f0ac30c 0000277e (.cinit..fardata.2.load) [load image, compression = rle]
9f0aea8a 00000002 --HOLE-- [fill = 0]
You can observe that the length of ".cinit..fardata.load" differs by significant value.
I have set --zero_init = on and --cinit_compression=off in project linker settings.
How can I apply rle compression for .fardata section only in CCS7
Regards,
Pradeep