Tool/software: TI C/C++ Compiler
Hello,
I'm using CCSV8 with V18.1.0 compiler.
In my program, I have some declared "enum" with only superior or equal to 0 values. So, the compiler defines automatically the "enum" as an UNSIGNED INT, isn't it?
But, according to my specifications, I have to test if the first value is well superior or equal to 0.
For all of this tests, the compiler displays a WARNING because the test is already right.
My question is: is it possible to disable the automatic definition of the "enum" and always treat "enum" as INT on the compiler (even if the first "enum" value is equal to 0)?
Thank you very much.
Best Regards,
Alexandre.