Tool/software: TI C/C++ Compiler
Hello,
Working on the DSP in The TDA2xx.
I am using compiler version TI v.8.1.0.
I keep getting semantic errors on the __int40_t type (it can still build but annoying)
The c6x.h is included but i did not see on that file any typedef for this type so i am assuming it is a compiler built in type.
Whats strange is that for the __x128_t type i dont get any errors from CCS / indexer.
Can you help resolve this?
in the meanwhile i had placed a "typedef long long _int40_t" under a CDT_PARSER #if
Thanks
Guy