Downloaded & installed Power Stage Designer 2.
It does not run.
I have the latest JRE installed as per the instructions.
The java path is correct in the XP environment variables.
Running XP SP3.
Nick
Hi Nick,
sorry for the delayed answer, I was on vacation.
Regards,Matthias
Hello Matthias,
apologies for the late response I've been on holiday too.
I resolved the issue with Power Stage Designer.
Yes I removed all previous versions of Java.
No error/pop up messages. The process just sat there. No windows, nothing.
Yes tried both exe & jar files. Didn't run. Something did as it appeared in the list of processe but that's as far as it got.
I fixed the problem as I had installed Java 7. I removed this.
Installed Java 6 rev 27 and everything appears to be running fine. Although Sun say this is Java 7 it actually isn't.
I had previously been running a beta version of Java 7 which Power Stage Designer doesn''t appear to run with.
Thanks.
sounds pretty tricky, but fortunately now it works!
Enjoy the program & best regards,Matthias
Hello,
I have a customer having issues opening Power Stage Designer with JRE 7 Update 4. Is the current recommendation to downgrade to the latest update of version 6 (currently update 32)?
Regards,Andrew Kling
We figured out that the Java API slightly changed. This will be considered in the next release.I've sent a hot-fixed version to Andrew which he can test with the customer.
A short-time solution could be a downgrade of JRE 6.
Thanks Matthias!