I'm attempting to us TI's provided LP5907_DQN_4.bxl file to import the DQN style footprint into Altium using Ultra Librarian and the footprint I'm getting does not match the datasheet. The footprint looks OK but it is if all the dimensions have been converted to imperial instead of metric. For example, the TI datasheet shows a 0.65mm center to center pad spacing but when I import it into Altium it measures as 0.65 inches. This is true for the whole part, everything that should be in mm is in inches, scaled properly but the wrong size overall. Is this a problem with how I am importing into Altium or is there possibly an error in the bxl file? I've imported before without having a problem.
Thanks