• TI Thinks Resolved

TINA/Spice/UCC28710: Flyback AC/DC simulation problem

Part Number: UCC28710

Tool/software: TINA-TI or Spice Models

Hi,

I built a AC/DC 5V/2A  flyback circuit with UCC28710 transient model, and its schematic is to duplicateevaluation board PMP9202 with simplified components in the input and output.

Some diodes and the primary side HV-MOS model was collected and put in the simulation.

But the simulation result shows the primary side HV-MOS could not be switched continuously that no output was found.

Attached are the result and TINA .TSC file, could anyone help take a look on this simulation ? I appreciate if there is any comment on this.

Thank you. 

Flyback_UCC28710_PMP9202.zip