This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TINA/Spice/SN74AUP1G14: TINA-TI Spice Model Available?

Part Number: SN74AUP1G14

Tool/software: TINA-TI or Spice Models

Hi,

Is there a TINA-TI Spice Model for the SN74AUP1G14? It'd be great if there were TINA-TI models for all of the Tiny Logic family, but I'm mostly interested in the SN74AUP1G14 at the moment.

Regards,

Jeremy

  • Hi Jeremy,
    I can build a behavioral model for the SN74AUP1G14 for Tina-TI. I will get that posted in the next hour or so.


    Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

    The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.

  • In reply to Emrys Maier:

    Hi Jeremy,

    Please see the attached model.

    I want to mention that this is a behavioral model -- it will act much like the device, but it is not 100% representative of the real device.  For example, you can input 100V to this device and it won't complain a bit, but the real device would fail spectacularly at that input :)

    If you find something that does not respond the way you would expect, please let me know and I can look into it.

    SN74AUP1G14_Behavioral_Model_v180518.TSC

    SN74AUP1G14.cir


    Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

    The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.

  • In reply to Emrys Maier:

    Hi Emrys,

    Thanks so much for creating a model for the SN74AUP1G14 that is compatible with Tina-TI. I'll take a look and let you know if I run into any problems.

    Regards,

    Jeremy

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.