TINA/Spice: Logic functions, D, XOR, Time delay

Tool/software: TINA-TI or Spice Models

Hi

I need a simple functional model for some logic functions - D type flip flop, XOR gate and a time delay (I need to be able to set delays from 100ns to 5us .

It would be nice too, if there was a square wave generator with a settable duty cycle (about 0.5%) - I'm using a Pattern Generator for that at present, it works but it's a bit of a kludge.

I haven't seen anything in the TINA libraries so is there a way I can implement these functions. I'm not worried about rise times, fall times and so on, just simple 1s and 0s will do nicely.

Thanks

Colin

1 Reply

  • Hi Collin,

    The inbuilt digital libraries are only available in the paid version of TINA-TI. We have some internal libraries in PSpice that can be used in TINA-TI. we can provide that to you. We will take this conversation offline so we can continue the discussion in detail. If need be, we will update here with final summary.

    Nikhil Gupta | Product Folder Modeling                                                                                                                                                    

    All TI Spice Models can be found here | All WEBENCH supported devices can be found here

    New to TINA-TI? Its a free spice simulator! Try out this short Video Training Series